7/3/2009 8:25 AM | |
Joined: 9/27/2006 Last visit: 6/26/2024 Posts: 12262 Rating: (2672) |
Hello lalit; The MSG instructionuses configured connnections to exchange data over AB networks, DH+, ControlNet, Ethernet/IP... Similar exchanges can be established with Siemens CPUs using S7 connections and instruction blocks, over Profibus, Industrial Ethernet and MPI. The following attachment is a page from the Simatic Communications manual, and discusses S7 connections and the SFBs/FBs that can be used to exchange once they are configured: http://support.automation.siemens.com/WW/view/en/25074283 The online help of Step 7 and the System and Standard Functions manual will give you more information on the spercified functions. Hope this helps, Daniel Chartier |
Follow us on