(1)| 1/17/2025 8:39 AM | |
|
Joined: 1/17/2025 Last visit: 10/16/2025 Posts: 2 Rating:
|
It's been a while that I was programming a Logo and now I'm facing a small challenge. I need to open or close a valve (powered by a hydraulig pump/cylinder). I want to put a digital positionsensor on it to get feedback of the actual position (4-20mA or 0-10V). I will type in the desired position into the screen and then based on the actual position either digital output "close" is activated or digital output "open" is activated until the values (my typed value and the feedback value) are the same then the digital output becomes inactive. Attached is the LSC, in the bottom is what I'm having trouble with. Thanks up front! BR, Peer
AttachmentVoedingslijn.zip (228 Downloads) |
| 1/17/2025 11:33 AM | |
|
Joined: 1/17/2025 Last visit: 10/16/2025 Posts: 2 Rating:
|
Thanks a lot!! |
Follow us on