(0)| 10/14/2024 8:58 AM | |
|
Joined: 4/20/2017 Last visit: 1/9/2026 Posts: 85 Rating:
|
Hello guys I have same problem + crashing. I have TIA Portal 18 Update 4 installed in VirtualBox Windows 11 64bit.. Without any warning I started to have issue to paste copied text.. For example if I copied variable from one of the ladder instruction and I want to paste it to another.. Or to past it to comment, then nothing is happening.. If I do that multiple time, than TIA crashes... Sometime helps if I start to type something, something random and then I paste copied text, it works.. But not every time.. And also coping from TIA to Notepad or whatever works perfectly fine. ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 10/14/2024 10:04:20New subject after splitting |
|
| 10/14/2024 2:05 PM | |
|
Joined: 7/7/2010 Last visit: 1/23/2026 Posts: 16409 Rating:
|
Submit a Support Request using the link in the gray bar above. |
|
science guy |
|
Follow us on