(0)| 2/24/2025 9:05 AM | |
|
Joined: 9/30/2016 Last visit: 1/12/2026 Posts: 953 Rating:
|
Please also see the attached screenshots. We have a machine with a G120_CU240E_2_DP_F drive. The drive was failing so we need to replace it. We are still using Simatic Manager and Starter 5.4 on most of our machines but are (slowly) moving to TIA. In order to be sure that the programming is not changed I want to first copy the programming from the drive to my PG. I connected my PG to the drive via a USB adaptor and managed to connect to the drive and follw the wizzard to copy the programming the my PG. Then the drive was relaced with a spare and I tried to download the programming to the new drive but was informed that a connection was not possible. When I search for the new drive in Starter i CAN find it it but naturally I don't want to copy from an "empty" drive. What am I doing wrong and how can I download the programming to the drive? AttachmentDrive SW.zip (273 Downloads) |
| 2/24/2025 9:20 AM | |
|
Joined: 5/12/2006 Last visit: 1/16/2026 Posts: 22827 Rating:
|
maybe wrong Profibus adress? Can you provide a screen what is displayed in accessible nodes? |
Follow us on