5/6/2025 2:14 PM | |
Joined: 7/1/2014 Last visit: 5/7/2025 Posts: 237 Rating:
|
Hi all, I am very confused about this... i did some research but i didnt expect it to be so "complicated". My need is simple. I need a Thermal Printer that is possible to mount on Panel. That will need to print some simple reports I create on the TP700 Comfort (just alphanumeric reports). I tried to use the compatktool but i find just a super short list of printers named Brightek. Can You please suggest me some printers that can do what i need? Thank You very much for the help in advance! EDIT: Let me add I will probably have to work with this:RS PRO Panel Printer | RS And looks like I cant use it directly via HMI... but i will need to send some instruction via PLC... |
Last edited by: dan.v. at: 05/06/2025 15:32:21 |
|
5/16/2025 6:36 AM | |
Joined: 8/3/2009 Last visit: 9/17/2025 Posts: 16447 Rating:
|
Hello dan.v. I´m afraid the only official information to printing options and released printer drivers from siemens for the Comfort Panels are in this Links: https://support.industry.siemens.com/cs/de/en/view/58205602 https://support.industry.siemens.com/cs/ww/en/view/11376409 I think also there will be no more development on this Panels. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on