(0)| 7/10/2009 9:06 AM | |
|
Posts: 261 Rating:
|
You did not mention the SP with the Sim. According to the SP of the PLC SIM it’s having with different options. What's new in S7-PLCSIM V5.4 incl. SP3 Multiple startability and communication support between the CPUsOptimization of the download scenario Support of an additional PG/PC interface: PCinternal (local) Simplified access path Optimization of communication with WinCC and WinCC flexible Display of all CPU access addresses in the status bar What's new in S7-PLCSIM V5.4 incl. SP2 S7-PLCSIM V5.4 incl. SP2 supports loading of configurations with "Configuration in Run" objects (CiR objects) during RUN mode.What's new in S7-PLCSIM V5.4 incl. SP1 S7-PLCSIM V5.4 incl. SP1 supports the group policy "Do not keep history of recently opened documents." S7-PLCSIM V5.4 incl. SP1 enables Windows Vista users to select an Ethernet CPU access node and use the ONLINE view of STEP 7 HW Config What’s new in S7-PLCSIM V5.4 DP, Industrial Ethernet and PC Internal connection types supported in addition to MPI Increased number of blocks supported for simulation. The attached doc gives you the SFB and SFC list supported by S7-PLCSIM V5.4 incl. SP3Regards ddg Attachmentsfb_sfc.pdf (611 Downloads) |
Follow us on