3/31/2022 9:14 AM | |
Joined: 8/3/2009 Last visit: 9/19/2025 Posts: 16452 Rating:
|
Hello bosandzeros there are a lot of things to consider: https://support.industry.siemens.com/cs/ww/en/view/88780011 If you work with VPN then you should use the enchrypt communication with a defined Port in Simatic Shell on both sides. Also you should use each other in the Simatic Shell as Multicast proxy. Check the Number of routers you have between the two stations and set the Multicast TTL to this value or higher. you must be able to see each other in Simatic Shell if it should work. If you do not get is work you can also use Plan B: https://support.industry.siemens.com/cs/ww/en/view/103198851 Bye Murof |
If this Information really helps, you could use the Rate function |
|
11/5/2024 3:45 PM | |
Joined: 8/23/2021 Last visit: 6/25/2025 Posts: 2 Rating:
|
Hi bosandzeros Regards |
7/22/2025 4:57 PM | |
Joined: 5/24/2018 Last visit: 8/13/2025 Posts: 1 Rating:
|
Does anyone have a solution to this? It is really getting to me now! Thanks |
Follow us on