8/21/2025 4:38 AM | |
Joined: 3/14/2008 Last visit: 9/17/2025 Posts: 2217 Rating:
|
Hi, This could be several things. If you line up the OS server on the ES station (not ES simulation), It would be best to remove the path to the target OS of the OS server (OS object). Also make sure the computer name is set to the ES station name, and compile the OS via TCP/IP for example (not named connections) and set the system unit for the s7 channel to PLCSIM afterwards. Checkmark: Alarm Logging Runtime must be set as well in the Startup list. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on