8/21/2025 5:38 AM | |
Joined: 3/14/2008 Last visit: 9/17/2025 Posts: 2217 Rating:
|
Hi, I do not know this folder, so I think you are correct. The OS project editor configuration can be edited so that the folder is included during configuration of the OS project editor. The OS project editor copies files from several installation directories and copies them to the project. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on