7/12/2009 6:42 PM | |
Posts: 178 Rating: (5) |
Greetings all, I am looking for a sample project WinCC to PLC controlling G130 drives. Many thanks, |
7/12/2009 7:46 PM | |
Joined: 5/28/2008 Last visit: 9/21/2024 Posts: 4515 Rating: (839) |
Hello, You can make your own code by insert the drive into the HW cong. and calling the associated addresses using telegrams. The following manual will be useful for you: SINAMICS G130/G150, List Manual, Valid for SINAMICS 2.6 SP1 Or using the pre-made FB14. You can download it from this FAQ: SINAMICS G Function block (FC14) to control an MM4 via Profibus-DP |
Ayman Elotaify |
|
This contribution was helpful to1 thankful Users |
7/13/2009 2:48 PM | |
Posts: 178 Rating: (5) |
Thanks for the info. |
Follow us on