8/22/2025 4:45 AM | |
Joined: 7/7/2015 Last visit: 9/2/2025 Posts: 58 Rating:
|
Hello Guys. I'm in trouble for time synchronization with NTP server. There's 4 PLC, and they get time from same NTP server. But all PLC's time is different. It seems the time synchronization is not working. I've set the IP of NTP server on CP 343-1 lean.(The gateway is set) (CP lean card : 173.2.220.xxx / NPT Server : 173.4.199.104) 1. The port from NTP server is opened for CP lean card. 2. I've tried to set the NTP server like it (https://www.industry-mobile-support.siemens-info.com/en/article/detail/22144502) 3. The ping test CP lean card <-> NTP server works well 4. I can see on the diagnostic, 'External error, incoming event' message. I have no idea what to do more. Is it caused by wrong setting of NTP server or network configuration? Could you help me please? AttachmentNTP asking.zip (22 Downloads) |
Last edited by: Ssung at: 08/22/2025 04:47:16 |
|
9/3/2025 11:45 AM | |
Joined: 8/3/2009 Last visit: 9/12/2025 Posts: 16409 Rating:
|
Hello Ssung Please check out the information in this FAQ: https://support.industry.siemens.com/cs/de/en/view/17990844 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on