9/3/2025 1:36 PM | |
Joined: 2/14/2023 Last visit: 9/10/2025 Posts: 1 Rating:
|
I'm using SetDAtaRecordToPlc to save the data from my recipe list to the plc, but i habe 2 recipe list that i want to send to the plc with 1 button. I have 2 SetDataRecordToPlc under the press event in the button but only the first one runs, when i switch them around it the firts one is the only one that works. I've tried it with VB scripts but then it also only runs the first one. How can i fix this? https://ibb.co/vCsttP2v < link to image |
Follow us on