9/11/2025 8:05 AM | |
Joined: 8/3/2009 Last visit: 9/17/2025 Posts: 16447 Rating:
|
Hello gaspar1 first to the PDF creation, it is possible to install a PDF printer on the Comfort Panels and this also works (I used it many times): https://support.industry.siemens.com/cs/de/en/view/58205602 you have two options to create some kind of datalogging to csv File: 1.) use the build in datalogging: https://support.industry.siemens.com/cs/de/en/view/109746939 you do not need scripts or anything special, you can just set everything in the TIA project. There is also a systemfunction for creating a copy of the logfiles if needed. 2.) If the datalogging do not fit your requirements you can also create own textbased files with scripts: https://support.industry.siemens.com/cs/ww/en/view/59604194 Of course you would habe to create the scripts by yourself and also you have to be careful with performance if this kind of scripts run too often or too fast...But it is fully custom Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on