(0)| 7/16/2009 8:39 PM | |
|
Joined: 10/17/2007 Last visit: 1/16/2026 Posts: 4579 Rating:
|
Hi, everyone I think it should not have F0001 after Factory reset when MM440 is in good condition I am sure my motor is good, and I have test more than 5 sets of MM440/MM430 after Factory reset and w/o motor connection, You should be able to start Fan running by BOP w/o any Fault. as I thought there must be something wrong with CPU card, so I searched and found in the Forum the post as following: /tf/WW/en/Posts/10618 as I metioned my MM440 isnot a newone. So I disconnected all connectors from CPU card to base board and connected again-----> the controller(my MM440) is OK now!! thanks for all of help from forum! |
Last edited by: nulizhang at: 7/20/2009 6:01 PMIf you like my comments please |
|
Follow us on