(0)| 7/24/2009 9:25 PM | |
|
Posts: 232 Rating:
|
Hi David. Please refer to the next link PROFIBUS DIAGNOSTICS Here you will find the FC125 and FB125, they are used to generate profibus diagnostics. Also you will find all the documentation you need to implement and parametrice those blocks acording on your needs. I hope this Help. Best regards. |
| 7/28/2009 9:55 AM | |
|
Posts: 28 Rating:
|
Hi. My CPU it's a 315-2DP(6ES7 315-2AG10-0AB0) andI see in the online help that the only 315-2DP compatible it's6ES7 315-2AF01-0AB0. |
| 7/28/2009 11:31 AM | |
|
Joined: 9/27/2006 Last visit: 1/21/2026 Posts: 12481 Rating:
|
Hello David; FB125 has been replaced by FB126 PNIODiag, and there is a link to the download page of that block in the earlier posts (although I would agree that it does not sound like a Profibus-DP diagnostiocs tool). Here however is the introduction to FB126from the download page: Description: The diagnostic package PNIODiag was generated in order to simplify the diagnostic evaluation of distributed I/O modules in connection with S7-SIMATIC. The diagnostic evaluation occurs for PROFIBUS DP systems as well as for PROFINET IO systems Your CPU model is part of the supported CPUs for FB126 (same download page); notice that there are 2 versions, and your CPU must use the one designed for CPUs with less than 16 kB storage options. Here again is a link to the download page: http://support.automation.siemens.com/WW/view/en/26996747 Hope this helps, Daniel Chartier |
Follow us on