4/10/2008 9:04 PM | |
Joined: 4/6/2006 Last visit: 2/5/2024 Posts: 604 Rating: (56) |
Hello Vadr, As far as I know the Logo isn't capable of doing AT Commands. But there is Insys modem available on for GSM communication with a LOGO! But if you need GPRS communication you can look at the SINAUT Micro System. It's based on the S7-200 and there is also aMicro Automation Set available. About those Micro Automation Sets is also a complete forum available:MAS Forum
|
Best regards, |
|
8/16/2009 7:40 PM | |
Posts: 1 Rating: (0) |
Please confirm that LOGO! does not support AT comands. I am looking for GSM modem, which I could connect with Logo! plc. INSYS gsm modem looks expensive. |
Follow us on