(0)| 8/24/2009 10:00 AM | |
|
Joined: 5/28/2008 Last visit: 1/22/2026 Posts: 4522 Rating:
|
Hello, First, I would like to correct the part number you have sent. The correct part No. is: 6SE6420-2UC15-5AA1 Second, The answer is YES, for sure you can run a 3 phase motor 240V from MM420, 1 phase 200 -240VAC. You have to conncet the motor "Delta connection" because in this case you will apply the output valtage (240 V) of the inverter on each winding of the motor. Please have a look on the following tip. Theory of operation of inverter from scartch Regards, |
|
Ayman Elotaify |
|
Follow us on