工业业务领域支持中心
Technical Forum
8/26/2009 9:36 AM | |
Posts: 22 Rating: (1) |
Hi, One way is to usemonitoring relay as 3UG, between G110 and the motor, and when current is reached, the 3UG give signal to G110 to trip. Regards, Angel |
8/27/2009 9:09 AM | |
Posts: 196 Rating: (12) |
Hi But can I get an Alarm / warning if the inverter detects the rotor is not turning. ? |
Follow us on