10/17/2009 11:16 AM | |
Posts: 59 Rating: (0) |
hello Friends, i'm using step-7 V5.4 sp-4 and wincc 6.2 sp-2. I have created the integrated WinCC in Step-7. Also i created the front end of WinCC same as PCS-7 front end. For this configuration everything works fine except alarm and trends. i'm facing a problem in alarm and trends is that: When i activate winCC everything works fine upto 10-15 min. After 10-15 minjust some thing happens like a refresh cycle for 1-2 sec, at that time all my containers disappear and again appear. When the container appears or after refresh cycle of 1-2 sec all my alarms aslo disappear.After that only the alarm color appears and no text. i have attatched the snap shot for ur refrence. In that case to view alarms, i have to deactivate and activate WinCC, then only the alarm text is displayed. once activated the same problem appears as explained above and again alarmdisappears. again to view alarms, i have to deactivate and activate WinCC. i aslo checked any settings for this, but i did'nt found any such setting. i have used the integrated back-up many time upto today, but i never faced such problem. this problem has become a very critical problem for me in plant, b'cozafter every 15 min i have to deactivate and activated WinCC. please suggest solution for this ASAP. waiting for ur reply. Regards, AMMU AttachmentWinCC alarm Problem.zip (48 Downloads) |
10/25/2009 6:26 AM | |
Posts: 59 Rating: (0) |
hello thanks once again Phantom 75 for ur reply. as per ur guidance, i'm sending you the WinCC diagnose file and also windows citamis.str file for your refrence. Waiting for your solution......... Regards, AMMU. AttachmentWinCC alarm Problem.zip (35 Downloads) |
10/27/2009 9:10 AM | |
Joined: 4/5/2006 Last visit: 4/24/2024 Posts: 917 Rating: (63) |
Hi Ammu ,
Again, you have problem with CCProjectMgr.exe application also how it is possible to see in PMDiagnose.log As well as Phantom75said "The date in alarms is also strange. What about the date when it is "working"? ": where that date coming from? from plc or yo are going to work on alarm databases with script?
if yes, problem should be in installation; if no, problem is your project
|
This contribution was helpful to1 thankful Users |
Follow us on