(0)| 1/11/2010 3:35 AM | |
|
Joined: 9/27/2006 Last visit: 1/21/2026 Posts: 12481 Rating:
|
Hello B. Prashant; Have you seen the following appication note from Siemens? http://support.automation.siemens.com/WW/view/en/22072988 Is uses a TP 117B along with a S7-300 CPU and Profibus to control a MM440 drive (also a Sinamics G120 ); it also has oprtions for Profinet. Now, the basic issue they are illustrating is start/stop control, but they also show how they change the value of one parameter in runtime, so you can extrapolate for your own project. Ihope you have already looked for information regarding the Profibus-DP telegram structure of MM 440 drives; hopefully the attachmed documentwill be worth studying. There are a few threads on the forum concerned with the same subject, you might want to search for them. Hope this helps, Daniel Chartier AttachmentMM4_PB_OPI_en_0202_I.pdf (318 Downloads) |
Follow us on