(0)| 1/21/2010 1:04 PM | |
|
Joined: 5/28/2008 Last visit: 1/14/2026 Posts: 4522 Rating:
|
Dear Cpt_KirK, Did you changed the parameter P1240 "Configuration of Vdc" ? Also please tell what is the application for this drive. And also please double check that the parameters of the motor has been inserted correctlly during quick commissioning. Do you have problems in the supply voltage? Specifically over voltage? Finally, Try to reset the drive to factory setting and then go to quick commissioning and enter the motor parameters and also select the command sources,...etc. And tell us what happened To reset the drive to factory setting, please follow the few steps in the picture. Regards, |
|
Ayman Elotaify |
|
Follow us on