2/4/2010 5:53 AM | |
Joined: 2/6/2009 Last visit: 6/18/2024 Posts: 939 Rating: (118) |
HiUMENCHO,Darius, Thank you for your suggestions. Now I am able to communicate with the meter, I want to know the data format of the Modbus communication in S7-200. The exact problem is, When I am reading 20 registers from the Modbus slave (as per the slave manual) I am getting the data's at the correctreceivelocation, But if I am changing no. ofqueries the data is not coming in the same location. Please helpme to find out the data structure format of S7-200.I have communicated the same meter in S7-300 by using CP-341 and it was fine. I want to know how to make Modbus program formore then one query in S7-200 plc's. |
Last edited by: O_Moderator at: 2/4/2010 11:30 AMnew subject after splitting from /tf/WW/en/Posts/39698#top _______________________________________________________________ |
|
Follow us on