3/19/2010 3:57 PM | |
Posts: 22 Rating: (1) |
Hi, to reverse motor without going through Stop use these parameters: p727= 1 Set function of theone of DI for set to [1] On/OFF1 / for example p701=1 Set function of the other DI for [2] On reverse/OFF1/ / for example p702=2 See parameter description for more information. To usefixed frequency: p1070=r1024 // main speed setpoint comes from fixed frequencies Select fixed frequency 1: p1020=0 p1021=1 p1022=0 p1023=0 The value of fixed frequency 1 by default is 5Hz which can be changed in p1002. For more information use Parameter list manual:
Regards, Angel Angelov |
Last edited by: abvto at: 3/19/2010 3:59 PM |
|
Follow us on