3/31/2010 10:07 PM | |
Posts: 48 Rating: (1) |
Hello, I could have multiple connections , with s7 cpu315 MPI, and s7 317 ethernet in the same project wincc flexible 2008 hf3 |
4/1/2010 1:39 PM | |
Joined: 4/24/2006 Last visit: 5/31/2024 Posts: 8664 Rating: (1154)
|
Dear aguere, It should be possible Perhaps this link might help: Why is the communication driver marked 'orange' in WinCC flexible when another ethernet communication is added to an existing MPI/DP? Best regards, Wizard |
Follow us on