4/28/2010 5:44 PM | |
Joined: 1/4/2010 Last visit: 5/2/2024 Posts: 650 Rating: (40)
|
Hi Which operating system do you have? Which software do you also have on your PC? I think it is a problem with the compatibility. http://support.automation.siemens.com/WW/view/en/21927773 |
Regards |
|
5/1/2010 7:28 AM | |
Posts: 6 Rating: (0) |
Dear Romulus Thanks for your reply.I am Using Windows XP SP2 as OS.WinCC 7.0 SP1 is configuration software.it is communicating through S5 155H using CP 525.I am not using any antivirus. So I am not able to locate which software is not compatible with WinCC. |
5/3/2010 8:58 AM | |
Joined: 1/4/2010 Last visit: 5/2/2024 Posts: 650 Rating: (40)
|
Hi Do you Header generate and compile all functions in Global Script? Have you any errors? Have you enough disk space? Are there any actions when the error come? Do you do anything or are there a lot of alarms in this moment? Have a look in the diagnostic fo WinCC. Info about this find you in WinCC Information System>WinCC Diagnosis or in the support http://support.automation.siemens.com/WW/view/de/22892165 |
Regards |
|
Follow us on