(1)| 5/22/2010 1:24 PM | |
|
Posts: 31 Rating:
|
In the topic of how to display the error of Micromaster on a HMI check the link here I just want to clarify the configuration of tags... here is the statement: Open the “Variables” window and configure it. Set the configured connection. Change the data type to WORD. The parameter for error messages is the address DB 947 DBW 0. The parameter for warning messages is the address DB 2110 DBW 0. The following applies: parameter number = data block number Does it mean if the error in r947 = F0001(Overcurrent) the address will be DB947.DBW1 and if r947 = F0085(External Fault) the address will be DB947.DBW85 ? the other question is, can i display alarms and warnings of 2 micromasters in a single HMI (TP277 for example)...can i just copy the discrete alarm made by library Micromaster_Wcf2008 and then make another tag for the other connection(for the 2nd micromaster)? tnx... |
Follow us on