5/30/2010 10:18 AM | |
Posts: 31 Rating: (2) |
What is the easy way to display the Alarm and Error codes of Simodrive611u(with profibus module) in HMI using WinccFlex. The PLC is S7-300 and the fieldbus is Profibus... Can I used With SFB53 "WRREC" (write record) transfer a data record with the number INDEX to a DP slave device component (Simodrive611u) defined by ID and with the SFB52 "RDREC" (read record) read a data record with the number INDEX from a component (Simodrive611u). I have a project before using this SFB in displaying Micromaster 4 alarms and error in TP277...this was a sample project PN_Read_r947_r949_en. There is also a sample project for Simodrive named "toolbox_120101"... using this FB 83 Simodrive control, but i only want to display the alarms and warning to make my program simple... Is it also possible for simodrive to get the alarms and warnings only? |
Follow us on