6/2/2010 11:09 AM | |
Posts: 3609 Rating: (29) |
Import of a Technical Question of an User Tusharwrote: Dear all, 1) I am using MC drive for position control. 2) I am facing the problem in Homing Mode -- Axis not running else Position and set up mode are OK 3)I am attatching the drive parameter list for the same. 4)I am setting the REF_ON cmd , Speed Referance , Bero I/p and Axis direction 5) Still the Axis is not running --- What may be the problem please guide me. 6) Please give me sample program for the homing mode. Thanks & Regards Tushar |
Follow us on