6/25/2010 12:33 PM | |
Posts: 173 Rating: (95) |
Hey all of these needing layout help! Check out this old link - let me know if you can still find it or get to it! http://www.microautomationconfigurator.automation.siemens.com/ It was done for the 0BA5 and not marketed very well, but it was a bit of fun to play with at the time! I hope that Siemens updates it for the 0BA6 and the new modules (like the TD). Have you seen the latest DVD of info that Siemens is handing out? I got one at Hannover Fair - IT IS GREAT! It has EVERYTHING on it! Check the attachment for the version number and ordering number on the back cover to bug your local Siemens person for one - they are free!) A whole lot of re-worked application examples (using the 0BA6 FB's), all the updates and service packs, manuals etc. What is also great is all the pictures buried on it - great if you need a good pic for a project or a presentation! There are also all the CAD .dxf drawings on it. It really is a valuable resource - like having the entire LOGO! internet site in your pocket - great for when youdo not have an internet connection - like at a customer. And best of all, Siemens wants you to copy and distribute this DVD as often as possible - give one to all your friends! AaaaarrrggghhhHHH!!! ("Have a nice day!") (Please 'tahnk', 'rate' or send valuable items by smoke-signal) |
6/25/2010 2:42 PM | |
Posts: 661 Rating: (123) |
Hi there, did you see the"SIMATIC selection tool"? Sorry, i could not link it (does not work), but i can show you how to get there: 1)Go to www.siemens.com/logo 2) All about LOGO! logic module 3) Catalog and ordering system online 4) Configurators I did not reallyplay with it yet, but it seems as if it supports lots of products, not only LOGO! Attachmentsimatic selection tool.pdf (410 Downloads) |
Follow us on