(0)| 7/12/2010 11:55 AM | |
|
Posts: 39 Rating:
|
Hello, I am using SCOUT version 4.1 SP4 HF1. During the installation of the software I had checked the option of installing CFC. The installation took place completely. But the option of "Inserting DCC charts" does not appear in the SCOUT software when I try to do so. I have attached screen shots to illustrate the problem in a zip file "DCCInstallProb". I uninstalled the CFC charts software through the Control panel and tried to install it again but to no avail. Also the structure of the software has chaged, as in Libraries and the Monitor option appear at the top rather than in the bottom. But the software functions properly which does not have DCC backup Please suggest what can be done in this case. Regards. AttachmentDCCInstallProb.zip (369 Downloads) |
| 7/13/2010 10:58 AM | |
|
Posts: 39 Rating:
|
Hello, The version of the CFC chart has been shown in the screen shot which is an attachment. I think that the DCC library has not been installed along with the installation as I am not able to see the DCC library. When I go to Option->Block Types and try to get the library it says that the library not present. Why was the DCC library installation skippped and if I have to install it now how can I do it? I hope this info is enough. Regards. AttachmentCFCVersion.zip (369 Downloads) |
Follow us on