7/17/2010 8:10 PM | |
Joined: 7/2/2008 Last visit: 9/25/2024 Posts: 928 Rating: (308) |
Hello Jesper, One is called bit message (You write the message text in HMI) and the other called message numbering in which you use some SFCs to trigger messages (Write the message text in STEP7). Briefly you can check the message system in Definitely you will have to read more and dig into both STEP7 and WinCC flexible help files. However I hope you find these FAQs helpful. 1- Best regards. H-H |
Last edited by: H-H at: 7/18/2010 10:12 PMI thought it was about S7-300 or S7-400 not S7-1200 since it was in general SIMATIC S7 conference. I''m sorry I can''t help you with STEP 7 Basic. |
|
Follow us on