5/17/2010 12:20 PM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2983)
|
Hello, this is an internal system failure. Can you post the diagnostic log of the device? Regards Christoph |
6/9/2010 5:15 AM | |
Posts: 8 Rating: (1) |
hello ChristophD, Thanks for ur help. I get Simotion Scout online with D445 to trace the diagnostic buffer, but I found when the problem occured, the scout went offline immediately, and the diagnostic buffer can not refresh in time, so i couldn't see any useful diagnostic infomation. In addition, I also use the service selector switch to (SIM/NCK) to write diagnostics data to the CF card when the problem occured. But i think the CPU has crashed that time and maybe can not perform this function correctly. But anyway, i have done this and you can find the DIAG data in the attachment. Maybe u can help to find some useful infomation for me. Thanks a lot in advance. AttachmentDIAG.zip (144 Downloads) |
Follow us on