2/18/2010 11:09 AM | |
Posts: 19 Rating: (0) |
Hello, I saw in another thread that in RCV_PTP I can use a pointer in bufer input like "P#DB110.DBX0.0 BYTE 10", Can I use a pointer in SEND_PTP function and which memory location are supported (M,L,I,Q etc) ? Thanks ! |
2/18/2010 1:24 PM | |
Joined: 5/28/2008 Last visit: 5/23/2024 Posts: 1343 Rating: (141)
|
Hi, should also be possible. But as buffer is only a DB allowed. No M, I or Q. |
2/19/2010 8:05 AM | |
Posts: 19 Rating: (0) |
Thanks !!! I've tried it and it's working !!!! |
Follow us on