9/5/2010 12:05 PM | |
Joined: 8/27/2006 Last visit: 10/22/2024 Posts: 719 Rating:
|
Dear All, I have a project where I connect a barcode reader to a PLC 224XP through port1 using ASCII communication. Port0 is used for a TD200 The program works fine, then if I switch the power OFF then ON after a few hours, a portion of the program stopps. This portion is responsible for processing the ASCII received stream.To make the program run again, i must re-download the program. It happened on time that I uploaded the program to re-download it, it gave me the error in the first picture. When I monitor, the screen shows what in the second picture. I don't understand where is the error. Can anybody help? Thanks
Attachmenterror.pdf (221 Downloads) |
The more you know, The more you know that you don't know |
|
Follow us on