9/16/2010 7:19 PM | |
Posts: 6 Rating:
|
Hello, I ask your help to solve a communication problem between a CPU 315-2 DP (master of the DP net) and two thermoregulator units Eurotherm 3504. The Profibus network has this structure : CPU315-2 DP : Master of the net (theCPU is in MPI Net with another CPU 314C/2Ptp). ET200M : Slave, with address 3. The ET200M has 1 8AI card (6ES7331, acquiring 8 Thermocouples). Eurotherm 3504 #1 : Slave, Address 11. Eurotherm 3504 #2 : Slave, Address 12. The DP net works correctly only with ET200M (I read correctly the temperatures detected from the thermocouple). I enclose a zip file containing the S7 project (it is without PLC software because we're testing the network, the gsd file and the thermoregulator configuration) and the gsd files of the Eurotherm 3504 Can you help me to solve this problem ? Thanks in advance Roberto Conte AttachmentAttached.zip (275 Downloads) |
9/16/2010 10:25 PM | |
Joined: 7/28/2010 Last visit: 8/31/2024 Posts: 184 Rating:
|
Roberto, Could you check the"Hardware Diagnostics" and "Module Information" under Diagnostic/Setting tab and see what the error is? Regards, Behnam www.sigmaprocess.ca/blog |
Follow us on