9/17/2010 8:10 AM | |
Posts: 6 Rating: (0) |
Dear Experts, Is have some problems integrating TIM modules in my SCADA application where i am using PCS7 on S7400 stations. I have to put in function a dial up connection between a S7400 station connected over MPI with a TIM43 standalone which has to collect data from2 remote S7300 CPU stationswith aTIM33 in racks. Is it even possible to use the Sinaut ST7 configuration tool for this? Because of the modifications that are necessary in OB1 and OB100 in order to initialize the communication for dial up (PCS7 generates its own blocks). If so, please let me know what is the solution and maybe give me some guiding lines. Thank you very much. Best regards AttachmentTIMs.zip (26 Downloads) |
Follow us on