9/20/2010 5:15 PM | |
Joined: 4/9/2010 Last visit: 5/23/2024 Posts: 222 Rating:
|
I get error 0xce when trying to connect from WinCC Flexible runtime to S7-200. If you want to establish communication using the PC/PPI cable, proceed as follows: Removing the PC/PPI cable driver
The problem I have is thet the PC/PPI interface shows in both lists: left and right. If I click on uninstall (there is no "Remove" button) the interface still stays in the right list. I tried the same after making sure none of the access points are assigne to the PC/PPI cable but had no luck either. Splitted from Connection between winCC flexible runtime and S7 200. |
Last edited by: adam_ski at: 9/30/2010 4:49 PMLast edited by: O_Moderator at: 9/21/2010 11:40 AMnew subject after splitting Last edited by: adam_ski at: 9/20/2010 5:16 PM |
|
Follow us on