9/24/2010 8:39 AM | |
Posts: 2930 Rating:
|
Hi, if the MM420 is controlled via USS protcoll fro a S7-200, then you get the speed as a feedback from the USS_CTRL Block. If not, then you have to scale the value from the poti. This can be done by your selve, or you can use the scale-Lib for S7-200. The Lib you can get here: http://support.automation.siemens.com/WW/view/en/27043396 Hope this helps Helmut |
Follow us on