9/29/2010 7:35 PM | |
Posts: 1 Rating:
|
I'm a new guy in PLC programer. I have a problem not clear about tip38b for S7-200. In the S-ITR ( scale interger to real) value at AIW.. is from 0 to 32000 with type word, please tell me how to convert type word to type interger ??? LD Always_On // Load Special Memory location 0.0 // to cause execution every cycle -R #OSL, #OSH // Subtract OSL from OSH, store in // OSH (de-scaled Output value) -I #ISL, #Input // Subtract ISL from Input but input is word not is int // ISL(de-scaled Input value) when I use the simulation for S7-200 for tip38b, I get the fault (file attach) Sorry if my english not good ! thanks Attachmentfault when simulation.pdf (249 Downloads) |
Follow us on