10/11/2010 8:35 AM | |
Joined: 10/22/2008 Last visit: 4/26/2024 Posts: 365 Rating: (5) |
I consider solving the problem with different PAC. PAC 3200 has RJ45 and protocl Modbus TCP and SEA TCP. So there should be no difficulties in connectiong and communicating PAC 3200 and S7 300 PN standards. Just choose hardware and proper I address? Why PAC 3400 has only Modbus TCP? There is again problem with connecting it with s7300 because as you said above S7 300 dont have Modbus libraries. Am I right? Is it possible to get info from PAC to PLC with ethernet SEAbus? Or S7-300 doesn't support that protocol? best regards Splitted from s7300 and PAC3100. |
Last edited by: O_Moderator at: 10/13/2010 9:54 AMLast edited by: O_Moderator at: 10/12/2010 9:23 AMnew subject after splitting Last edited by: Oscar_83PL at: 10/11/2010 12:11 PM |
|
10/13/2010 10:43 AM | |
Joined: 9/22/2010 Last visit: 12/13/2023 Posts: 225 Rating: (28) |
Hello Oscar, there are libraries that you can use to communicate between S7 300 and PAC3200. You can find them at www.siemens.com/s7modbus Regards Sakura |
Follow us on