10/11/2006 12:24 PM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating: (151)
|
[quote user="alfie"] 1: when i open ur screen, i encounter with "error while openning document" ... P.S. i'm using wincc6 sp 2 I am using SP4 which is why you cannot open the pictures. You cannot go back from SP4 to SP2 as explained here. Can anyone put together a quick SP2 example ?? I'm afraid I don't have a SP2 machine with me today. If no-one responds I should be able to do sotomorrow or Friday. [quote user="alfie"] 2: in teh picture function wizard, i cant see "Picture Change in the Window" i attached all that available there! Ah, of course you are using PCS7 and/or BPC. Use the wizard "Change picture in workspace" as I think it does the same thing. The wizard should look like the attached picture. |
10/14/2006 7:28 AM | |
Posts: 78 Rating: (3) |
Sorry guys, I didn't access to internet last 2 days, I'll check this out and share u my problems.[;)] thanx a lot |
Follow us on