11/9/2010 3:47 PM | |
Posts: 7 Rating: (0) |
Ok guys heres my problem. I was under the impression that I would be able to make a [FC] then add to my library and use when ever I needed the block. I built a [FC] that simply turns on/off output based on 4-20 ma. I then draged this to my library, because I have several 4--20 instruments that protect a pump I was hoping to drag the element as many times as needed for each instrument Even though the block gets renamed everytime I use it, I get ambigious address when I compile and download. I will attach a small sample file. Thanks all AttachmentANALOG TEST STATION.zip (644 Downloads) |
11/9/2010 5:24 PM | |
Posts: 7 Rating: (0) |
huggy_d1 Thanks that worked great. Also thanks for the quick reply |
Follow us on