11/18/2010 8:35 AM | |
Posts: 13 Rating:
|
Hi, I have the same problem as Bilal Moolla. I use Step7 v5.4 SP5. I use S7-300 (315-2PN/DP). I copied PNIODiag blocks v1.7 (kleiner 16 KByte) into my project. When I type in SCL PNIODiag.DB126(); and try to compile it then I get error Non-existent function block or missing instance declaration. Please can you help me? Splitted from In my WinCC Runtime, I get an error code of: 1300 8082. |
Last edited by: O_Moderator at: 11/19/2010 8:41 AMnew subject after splitting |
|
11/19/2010 8:44 AM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating:
|
Thread closed, because question is already published in the following thread FB126 non-existent function block or missing instance declaration in SCL. Best regards O_Moderator |
Follow us on