(0)| 1/4/2011 3:24 PM | |
|
Posts: 14 Rating:
|
dear guys. I need your help.rr I've failed open profibus communication between D425 and PLC300 CP342-5 last time by using so-called "i-slave", but when I use the DP/DP coupler(D425-DP/DP coupler-CP342-5), It works well. I know there is another way to open profibus communication. it is a "GSD file". I just tried to do it with GSD file(Si0280ab.gsd), but It did not work well. TT In the manual, it was explained too simple. Please, check the below attchment and help me! AttachmentPLC-D425.pdf (535 Downloads) |
Follow us on