1/14/2011 9:27 PM | |
Joined: 9/27/2006 Last visit: 9/15/2025 Posts: 12408 Rating:
|
Hello pietpoerrie; It is hard to say at first glance if it is possible to communicate to a device that transmits on 9-bit frames, PPI is usually 10- or 11-bit standard. The following link will bring you to a FAQ on S7-0200 Tips and Tricks, a collection of S7-200 typical applications. Download the complete file from the link at the bottom of the page. http://support.automation.siemens.com/WW/view/en/1232912 Inside the files you will find sample programs where the s7-200 interacts with barcode readers and other serial equipment over the PPI cable, so at least you woill see how it is done. Hope this helps, Daniel Chartier |
Follow us on