3/10/2011 6:30 PM | |
Posts: 13 Rating: (0) |
Hi, (New to this!) I have written a small program to be viewed on a HMI but don't own one yet. Can the graphics be simulated on Portal? |
3/11/2011 9:12 AM | |
Joined: 4/24/2006 Last visit: 10/14/2024 Posts: 8745 Rating: (1168) |
Dear Jambo, First of all, a warm welcome. The answer to your question is: You can simulate a HMI. See this link: Why isn't communication between the Runtime simulation and the S7-1200 not possible if the PG/PC interface is not set correctly? And see this thread: /tf/WW/en/Posts/34588 But you can not simulate the S7-1200 plc. Best regards, Wizard |
3/11/2011 11:31 AM | |
Posts: 13 Rating: (0) |
Dear Wizard Thanks for the advise, it worked Jambo |
Follow us on