11/16/2006 3:53 PM | |
Joined: 4/24/2006 Last visit: 6/6/2024 Posts: 8673 Rating: (1158) |
Hi Jeebs, This can be done using Any pointers. You'll have to declare them yourself. I think the following faq can help you: http://support.automation.siemens.com/WW/view/en/2738030 Best regards, Wizard |
11/17/2006 8:43 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (316)
|
Hi Jeebs, See theSTL source to do something with the ANY-pointers for SFC20. In the help of STEP7 are the ANY-pointers described very well, so you have to fill the ANY-pointer by yourself, it is not difficult, but you have to understand what you are doing...... To read in this source, please go to your source-container in the program container and push the right mousekey and insertthe STL source {first unpack the STL from the ZIP}. When you import the block then first give ablocknumber to the FC"CopyDBxx" in the symbolik editor. "BLKMOV" have to be recognized automatically when you then double click on the source and compile the block. AttachmentCopyData.zip (444 Downloads) |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on