3/28/2011 9:41 AM | |
Joined: 9/20/2010 Last visit: 9/1/2021 Posts: 4 Rating: (0) |
Hello, I need s7 1200 example for quadro encoder (signal board) and sheme conection. |
3/28/2011 12:20 PM | |
Joined: 9/20/2010 Last visit: 9/1/2021 Posts: 4 Rating: (0) |
Hi. A,B end R signal |
3/29/2011 10:49 AM | |
Joined: 9/20/2010 Last visit: 9/1/2021 Posts: 4 Rating: (0) |
I have linear encoder LS486 and interface sin/cos to TTL, I need count up and down and if posible use R signal.
Attachmentls486c.pdf (599 Downloads) |
3/29/2011 1:00 PM | |
Joined: 9/23/2005 Last visit: 7/2/2024 Posts: 4347 Rating: (1439)
|
Hi, the encoder wiring is descript in the manual of the S7-1200 in the HSC description (page 109). SIMATIC S7 S7-1200 Programmable controller |
Denilson Pegaia |
|
Follow us on