4/8/2011 10:56 AM | |
Posts: 12 Rating: (0) |
hi, I am using simovert masterdrive with profibus connected to compact logix. When i set P554.1 to 3001 and P734.1 to 32, i am unable to start the drive when i set control bit 0 to 1. i get 008 (On Lockout) on the PMU. I can start the drive from the PMU, when P554.1 is 2100 and also when P734.1 is 33 but my Run bit in status word does not come on. what could be the cause of this? Splitted from What is OFF1, OFF2 and OFF3. |
Last edited by: O_Moderator at: 4/8/2011 1:51 PMnew subject after splitting |
|
4/8/2011 1:52 PM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating: (135) |
Thread closed, because question is already published in the following thread Starting Masterdrive through profibus . Best regards O_Moderator |
Follow us on