5/28/2011 1:01 PM | ||||||||
Joined: 3/21/2006 Last visit: 10/7/2024 Posts: 10229 Rating: (1181)
|
You should configure the connections in S7-400 CPU - in both H CPUs and using the example from my post above. There have S7 connection TCP/IP protocol
|
|||||||
5/28/2011 1:17 PM | |
Posts: 50 Rating: (1) |
Hi |
5/28/2011 1:21 PM | |
Posts: 50 Rating: (1) |
hi Thanks for the reply the uploaded file is exe file how to open the same in step7 project |
5/28/2011 1:27 PM | |
Posts: 50 Rating: (1) |
hi, i am transferring around 200bytes of data through ethernet communication which blocks are compatible for the same |
5/28/2011 1:31 PM | |
Joined: 3/21/2006 Last visit: 10/7/2024 Posts: 10229 Rating: (1181)
|
Double click and follow the steps there. The idea is unpack the containing of the file in selected folder and then in Simatic Manager select it and open the project... Info about quantity of transfered data and descriptions of used blocks you could find from there How do you configure a specified and an unspecified S7 connection for data exchange between S7-300 and/or S7-400 by way of Industrial Ethernet CPs? best regards, Hristo Mihalev |
Last edited by: UMENCHO at: 5/28/2011 1:42 PM |
|
5/28/2011 1:44 PM | |
Posts: 50 Rating: (1) |
hi thanks for the reply i had opened the backup whether getput blocks are compatible for the 200 bytes of data transfer |
Follow us on